Hello,
I have an application which uses the ADS1278 converter with a 25MHz clock input running in high resolution mode. According to table 8 on the datasheet the data rate will be 48.828kHz and the frame sync period should be set to 20.48uS. However, on this application the frame sync period is set to 25uS. I need to understand what the implications are from setting the frame sync period longer than what is prescribed by the datasheet. Will the data from the ADS1278 be corrupted in this scenario?
Thanks,
Kerry