Other Parts Discussed in Thread: ADS62P49
I have a recently purchased TSW1400EVM I am testing with an ADS62P49EVM as described under section 4.2 of the High Speed Data Converter Pro GUI users guide.
I configure both boards as described with the appropriate power, clk and input sources but I notice when I load the firmware for the ADS62p49_cmos option all of the user LED's do not light as described in the document. User LED 3 and 4 (D5 and D6) do not come on. More importantly when I setup the GUI as described and perform a capture I get an error "Read DDR to file TIMED_OUT_ERROR Time Out error" could you please provide me with information on how to proceed to trouble shoot this issue further.
On the status line in the GUI I see "Start ADC to GUI", then Read DDR to file immediately followed by a pop up window with the error above.
I'm running v4.00 of the software, version 0.2 of the firmware, the board serial number is KS692250, Interface type set to CMOS_LSB_0SKP.
Thanks,
Larry