Other Parts Discussed in Thread: LMP91200, ADC141S626
hi sir,
i use lmp91200eval to measure water ph with a ph probe.
i encouter a issue when reading adc141s628.
that is i can't read negative value from adc141s628. the lowest value of adc141s628 is 0,no negative value is got.
when i calibrate with ph4 buffer,values read from adc141s628 are positive,and these are correct.(i think so.)
when i calibrate with ph7 buffer, values read from adc141s628 are around zero,but never under zero.
when i calibrate with ph10 buffer,values read from adc141s628 are all zeros.(<- this is wrong,invalid.)
i read spec of lmp91200,adc141s626,LMP91200EVAL_REV0p7, and try to make it right,but i failed.>"<
Could you give me some suggestion about this situation?
bty,all paramters follow spec. of lmp91200.pdf,page 21 Table1 Configration register of PH measurement
i check voltage of several points,
LMP91200 vdd=3.3v,VREF=2.5v, VOCM=1.25,VOUT~1.25V
adc141s628 VA=5v, VIO=3.3v, VREF=2.5v,
VOUT-VCOM= 0.15v as ph4 buffer is used.
VOUD-VCOM= -0.15V as ph10 buffer is used.