Hi ,
I am using ads1299 to measure ecg signal, but it seems that there is much nosie and interference.
1) power line interference is huge
2) when people walk around me, there is huge interference
3) when stretch the cable between the electrode and the board, there is huge interference
For the bias electrode, I used JP6 to get the voltage generated by a voltage divier on the board;
For the reference 'SRB1', it is directly from the body (JP8) and then given to all the negative inputs of each channel.
Why is it like this? Thanks!
Best,
Qi