Dear Sir
I use the init code from AFE4403EVM Firmware Source v2.2 ,but the ADC_RDY pin come only one time on my board .
I have debuged it , it only is generated after the reset ,then there is not generated always.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Dear Sir
I use the init code from AFE4403EVM Firmware Source v2.2 ,but the ADC_RDY pin come only one time on my board .
I have debuged it , it only is generated after the reset ,then there is not generated always.
Hello Banggeng,
Did you check for the following?
1. Probe the ADC_RDY signal on the oscilloscope and check if the ADC_RDY signal occurs at every PRF.
2. Verify the AFE register configuration after the first ADC_RDY?
3. Probe the RESETZ and AFE_PDNZ signal and check the status.