This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TSW1400EVM, Application report SLAA545

Other Parts Discussed in Thread: DAC3482, ADS4249, CDCE62005

I am attempting to replicate the setup in the application report SLAA545 to setup a repeater application using the TSW1400EVM along with the ADS4249 and DAC3482 evaluation boards.  I previously downloaded the firmware project from this forum and now am trying to program the Stratix IV device on the TSW1400.

Is this accomplished with the JTAG port or is there a configuration option in the High Speed Data Converter Pro v4.00 software?.

If it is using the JTAG port an the USB blaster can you give me some information on how to configure the jumpers on sheet 21 of the schematics of the TSW1400EVM to use the JTAG port.  Also if this is setup can you give me some information on how you setup the various registers on the DAC and ADC evaluation boards as well.  It looks like it would be possible to setup the jumpers on the ADC board to configure it but I'm not sure what I need to do on the DAC board.

Thanks,

Larry

  • Hi Larry,

    The firmware can be downloaded to the TSW1400 through HSDCPro. After connecting to the TSW1400, you can go to "Instrument Options" and select "Download Firmware". You'll then be able to select the desired firmware. Note that custom firmware (including this one) will not be functional in HSDCPro outside of downloading the firmware.

    The JTAG port can be used to download the firmware as well, however there are a number of resistors that will need to be removed and installed. You can find the schematic on the TSW1400EVM product page under "Design Files". The JTAG connector (J13) is on page 21. There are eight resistors that must be installed (R129-R132 and R57-R60) and another 4 that have to be removed (R61-R64). An Altera programming pod can then be used to interface directly with the FPGA using their software.

    Regards,
    Matt Guibord
  • Initially I got a message that no firmware was loaded when I tried this.  I noticed that the .rbf file generated when I compiled the ads4249_dac3482 project was not the same size as the other firmware included for the TSW1400, this was due to the project having compression set.  Once I removed that and attempted to program the FPGA with the correct size .rbf file I got the same message that it did not load but see that the LED's are consistent with the firmware being loaded.  I can see the LED's respond accordingly when I press reset so I know that it did load.

    The rx pll shows it is locked based on the LED's and the configuration of the ADS4249 appears to be fairly simple with the jumpers.  I have it set in BIN LVDS mode with the jumpers.  I'm running the DAC3482EVM Software Control through the USB interface to set the DAC3482EVM registers.  A configuration file would be helpful for the DAC3482EVM so that I can load the registers with the appropriate values for this example.  It does not appear that I can set things like interpolation with any jumpers on the board. I can see that it comes up with x8 interpolation instead of x4 along with the input FIFO enabled, I'm not sure how the FIFO was set up for this example.  Also the registers and settings for the CDCE2005 have capacitance and resistor values with no information on what they should be.  Any information you can give me on how the registers and values were setup on the DAC3482EVM for this example would be helpful.

    Thanks,

    Larry 

  • Larry,

    The DAC3482 EVM config for the project requires an external 1GHz clock source to the clock input SMA port of the EVM. The on-board CDCE62005 divide the input clock by /4 to provide the reference clock to the FPGA.

    The attached config file configures the DAC3482 EVM to 4x interpolation, FDAC = 1GSPS, FDATA = 250MSPS, FPGA_CLOCK at 250MHz.

    Additional DSP path on the DAC3482 such as NCO, QMC gain/phase, and QMC offset were NOT enabled.

    See attached

       x00	   x028C
       x01	   x0000
       x02	   x8002
       x03	   xA001
       x04	   x4DF1
       x05	   x0000
       x06	   x3400
       x07	   xFFFF
       x08	   x0000
       x09	   x8000
       x0A	   x0000
       x0B	   x0000
       x0C	   x05A6
       x0D	   x05A6
       x0E	   x05A6
       x0F	   x05A6
       x10	   x3000
       x11	   x0000
       x12	   x0000
       x13	   x0000
       x14	   x0000
       x15	   x0640
       x16	   x0000
       x17	   x0640
       x18	   x205F
       x19	   x10F4
       x1A	   x4820
       x1B	   x0800
       x1C	   x0000
       x1D	   x0000
       x1E	   x1111
       x1F	   x8882
       x20	   x2400
       x22	   x1B1B
       x23	   x001F
       x24	   x1000
       x25	   x7A7A
       x26	   xB6B6
       x27	   xEAEA
       x28	   x4545
       x29	   x1A1A
       x2A	   x1616
       x2B	   xAAAA
       x2C	   xC6C6
       x2D	   x0004
       x2E	   x0000
       x2F	   x0000
       x30	   x61A8
       x7F	   x0001
    CDCE62005 Registers
    Freq:19.200000MHz
    Address	Data
    00		80400000
    01		813C0001
    02		81400002
    03		C1840003
    04		C1840004
    05		29F01A55
    06		44AF0006
    07		165294A7
    08		20001808