Other Parts Discussed in Thread: ADS1248, TPD1E10B06, TPD2E001
Dear engineers.
I have ADS1248 connected as totaly insulated from microcontroller (we are using LM3S2793 now, but we going to change to STM32Fxx).
Everything is OK until I start BURST test to input wires. If testing voltage is large then -1200 V ADC stops converting (result is 0x7FFFFF).
If I set all 13 configuration registers to original values, which I have stored, function is restored and ADC continues work.
I reload registers after reading each measured data.
I check EVM schematics and I change C69 and C68 to 10 uF, It was without visible result.
Please, tell me, how make construction more robust and highly resistant. We need works in Class A (without lost of functionality).
Thank you
Jiri