I have been working to setup the SPI interface between the AMC7836EVM and the MSP430F5438A Experiment board, but it wasn't successful in the configuration process and wirte/read data.
i want to know if there exists a configuration secuence.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I have been working to setup the SPI interface between the AMC7836EVM and the MSP430F5438A Experiment board, but it wasn't successful in the configuration process and wirte/read data.
i want to know if there exists a configuration secuence.
Hi:
informando que encontramos el error en nuestro codiigo, al bajar el CS bajabamos todos los pines de ese puerto lo cual creemos que afecta a los pines del SPI que se utilizan en ese puerto.
Tengo otro problema al momento de leer esta tarjeta, al estar realizando un debuggeo con la tarjeta, no obtenemos respuesta alguna por parte del AMC. Pero al realizar una prueba desconectandoo el JTAG y con el CLK del MSP430, la tarjeta AMC responde sin ningun problema, quicieramos saber el motivo del problema
Hi,
For your information we have found out our issue in our code , while downloading the CS, we disabled all the pins from that port. which we belive that it afects the SPI's pins that the SPI uses on that port.
We have another problem, at the moment of reading the ACM, while debugging the MPS, we do not obtain any response from the AMC, But if we perform a test by disconecting the JTAG and with the CLK from the MSP430, The AMC responds with no issues , we would like to know the root cause of the problem.
Thanks & Regards.
Howdy Ivan,
If using on-board supplies:
When using J7 header with an external microcontroller, please ensure that VDUT gets connected to the micro-controller supply (3.3V). VDUT not only generates the IOVDD supply for the device, but also acts as an enable signal to turn on the TPS voltage regulators located on the EVM. When this power block is active, and wall wart connected, the regulators will produce all supplies required by the AMC7836 device. This includes the +12V, +5V, and -12V supplies. This can be verified by the D2, D3 and D4 LEDs, which will be on.
If using external supplies:
Optionally, if supplying IOVDD through J9, and not VDUT, all supplies must be connected to external sources through their respective terminal block. Also verify that VDUT is not connected to any voltage.
Regarding the JTAG and MSP430 Connection:
Best Regards,
Matt
A copy of the EVM schematic can be found at the following website: