Other Parts Discussed in Thread: DAC37J84, LMK04828
Is this the correct procedure for synchronizing two DAC37J84 EVMs (call them A and B) connected to
the two high pin count FMC connectors on the Xilinx Virtex 7, VC707 eval. card.
Referring to the DAC37J84 EVM schematic, seems like the following steps are needed:
1. Remove R16 and R18 from EVM A (This disconnects the LMK 04828 DACCLK).
2. Connect J1 and J3 on EVM A to J1 and J3 on EVM B (drives DACCLK from B to A)
3. Remove R4 and R7 from EVM A. (This disconnects the LMK 04828 SYSREF).
4. Connect J5 and J7 from EVM A to B (drives SYSREF from B to A)
Now EVM B is controlling DACCLK and SYSREF on EVM A
The FPGA will need LMK04828 DCLKOUT0 on FMC B to synch the JESD204 timing
Does this seem correct? Has anyone actually done this?
Thanks very much, John Reyland