Hello,
I have proven that with the AFE4403 EVM GUI I'm able to modify some of the AFE4403 parameters
Thus, I have two questions:
1. How can I record the HR signal, for example during 2hrs? Which parameters should I change?
2.Due that my purpose is to use the device without the GUI, being the user who decides when starts and stops recording the signal, ie controlling the state machine, how could I modify the LED that is measuring the signal or the gain of the TIA?
Best regards
Rocío.