This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AFE4403 Watch EVM accelerometers

Other Parts Discussed in Thread: AFE4403

Hi,

It appears that the default firmware for the AFE4403 Watch EVM doesn't give access/collect any data from the accelerometers which are part of the EVM hardware. Is the only way to access the outputs from these accelerometers to write a custom firmware, or is there an alternative approach?

We want to assess the AFE4403 performance under motion, but can only do this if we've got the accelerometer signals to use to clean up the PPG trace.

Thanks in advance for your help.