Hi,
I have some doubts about the real data rate of each channel of ADS12929R, can someone please confirm my understanding about this issue. When the data rate is set to e.g. 125 SPS in the device, this means 125SPS for each channel, right? If so, the bandwidth of the signal would be 62.5Hz. As stated in the datasheet, in this case the cut-off frequency of the digital filter is 0.262 * fDR which would result in 32.75, meaning that the bandwidth of the final output signal would be 32.75 Hz, right? Am I making mistake about anything here?
Actually, I fed a couple of sinusoidal signals to the device, took the signal to MATLAB to see the frequency characteristics of them, and noticed that 125 is the correct data rate for one channel (frequency peaks were at the correct locations). I also tried to see if there is any attenuation after 32.75Hz in the signal but I didn't notice any.
I would appreciate if anyone can clarify this for me.
I also took a brief look at the TI's two documents about delta-sigma ADCs, but I didn't find the answer of this question.
Regards,
-Vala