Hello,
Our customer uses DAC8760.
When they use following conditions,it flowed overcurrent.
- AVDD : 24V
- They are referencing Figure88 of datasheet(Boost Mode Configration).
- output current range : 0mA to 24mA
When they connected directly Ammeter without registor to IOUT pin,
the current increased to 100mA from 24mA.
Transistor was broken at the same time.
When the current increased,that is occured nothing in Status Registor.
And it wasn't output of the signal from ALARM pin.
They connected thermal PAD to GND plane.
Could you please tell me the cause of the over-current?
If you want to confirm detail,I have a circuit diagram of a customer.
So I can send at E-mail.
Best regards,
Manabu Ito