Other Parts Discussed in Thread: ADS1220
I use the ADS1220 to read type B thermocouple.
The Type B output is extremely low at low temperature (30 microvolts @ 100 deg C), which
necessitates averaging for filtering.
While the 1220 can sample at 1000 SPS at the background, for practical temp reading 20 SPS is more than sufficient.
The question is if anyone knows if there is a way to make the 1220 read and internally average at 1000 SPS, while the program reads at
lower rate (20 SPS or even single shot per call), or is there another device that can do it?
It seems a real waste if this is not possible, as the 1220 could provide the averaging at the background at no cost.
Samtal