Hello,
I have a board using DAC3482 and i am able to generate signals with it.
I would like to change the QMC I and Q gains (config12 and config13 respectively) while dac is generating.
I have noticed that i can write in config12 and config13 but nothing changes in the analog dac outputs.
Should i follow the complete power -up sequence if i want to adjust a register?
Please advice.
Dimitar Penev