Dear Sir or Madam,
We are developing a set of data acquisition system with ADS1281. Software and hardware are ready in the test phase now, but some problems are found during the test, so we need some technical support about the situation.
1、We input a fixed signal at the input terminal, run the software and print the output data. Some irregular sudden jumps are found in the output data.
The output data is as follows
( nine channels AD test data, channel 2~9 are shorted, and channel 1 is fixed voltage input; unit: MV)
Channel1=127.386521
Channel1=127.249569
Channel1=127.310352
Channel1=127.383909
Channel1=127.345219
Channel1=127.498473
Channel1=127.304534
Channel1=124.137772
Channel1=127.364546
Channel1=127.473443
Channel1=127.416875
Channel1=127.366232
Channel1=127.390288
Channel1=127.041611
Channel1=127.098906
Channel1=127.173799
Channel1=127.160172
Channel1=127.288516
Channel1=127.359855
Channel1=124.134092
Channel1=127.476981
Channel1=127.510580
Channel1=127.222052
Channel1=127.148076
Channel1=127.109911
Channel1=127.076918
Channel1=127.320980
Channel1=127.323648
Channel1=127.335932
Channel1=127.337407
Channel1=127.514082
Channel1=127.499506
Channel1=127.233353
Channel1=127.072852
Channel1=127.067674
Channel1=123.945175
Channel1=127.091292
Channel1=127.107072
Channel1=127.306097
Channel1=127.267259
Channel1=127.167264
Channel1=127.316280
Channel1=152.818520
Channel1=127.350961
Channel1=127.266604
Channel1=127.258757
Channel1=124.101284
Channel1=127.240173
Channel1=127.267108
Channel1=127.234491
2、The SCLK and DRDY pins of the ADS1281 are connected to the oscilloscope, which has curves as below, showing a number of sudden jump pulses signal superimposed on the DRDY. Is the previous sudden jump in the data caused by this sudden jump pulses?
3、When we test the ADS1281EVM by the same method ,the output is the same. So we want to know if the demo board can be stabilized to 1 micro-volt by itself, if not, how can we improve the stability of it to 0.1 micro-volt or 1 micro-volt?
Best regards,