Hello,
I use the ADS1296 as following:
Internal ref: 2.4V; Analog Vdd: 5V; Digital Vdd = 3.3V; LP mode; 250SPS
I use channel 3.
INN3 = gnd and INP = 1.04V. Input: normal IN.
Either in RDATA and RDATAC I have the following weird results:
Gain = 1 => Channel3 value = 1.0474V (0x37DD0D) => OK
Gain = 2 => Channel3 value = 1.3962V (0x4A7685) => Why not 2V????
What am I wrong?
Best regards
Michel