I would like to generate two identical (or as identical as possible) signals out of DAC A and DAC B of the DAC3162, that is same amplitude, frequency and phase, so they are a replica of one another basically, or at least as close as possible. Is it safe to assume that this DAC3162 will output the samples at approx. the same time?, even though they are taken at its inputs at different times (interleaved)?, if so what is that maximum difference I should expect between the two if not negligible. The maximum frequency I am interested is 10MHz.
Thank you