Hello,
I have installed the firmware provided by TI in “www.ti.com/.../slaa671”. The AFE4403 Watch HREVM Works correctly. I have developed a program to get AFE4403 data from USB serial port but now I don’t know how to interpret the information.
The info adquired looks like this:
Line: 30 32 30 31 ff e5 cf 05 f6 01 01 df 00 a5 0f a8 37 00 30 33 30 61
Line: 30 32 30 31 ff e5 ea 05 ed b3 01 bb 00 b2 0f c2 37 00 30 33 30 61
Line: 30 32 30 31 ff e6 05 05 e5 05 01 94 00 bb 0f d1 37 00 30 33 30 61
Line: 30 32 30 31 ff e6 03 05 dc 6b 01 5c 00 af 0f d6 37 00 30 33 30 61
Line: 30 32 30 31 ff e5 f2 05 d7 1d 01 6c 00 af 0f db 37 00 30 33 30 61
I think the first 4 bytes are a header and the last 4 bytes another header to indicate the init and the end of transmition, but I need to know what are refering to the rest of the bytes. Where is the PPG info?
Thanks in advance,
Rocío Camíns