Hi,
I would like to ask you some basic questions about DAC3xJ82 as below.
Q1) Bypass internal Mixer
Is it possible to bypass internal signal processing circuits (Mixer, etc)?
That is to say, I would like to get the outputs which are D/A converted from direct input data.
Input data (JESD204B) ----> No processing (Bypass processing) -----> DACOUT
Q2) OUTPUT channels
If Q1 is yes, is it possible to get 4 ch outputs (A, B, C, D) independently?
Normally, A and C ch are I data of 1 and 2 ch, B and D ch are Q data of 1 and 2 ch, I think.
Q3) Evaluation environment
TSW14J56EVM board is necessary to do above evaluation?
For example, how about "Signal Generator of JSD204B + DAC3xJ82EVM" is possible to evaluate?
Thank you very much in advance!