This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADC - strictly managing sampling timing

Guru 19785 points

Other Parts Discussed in Thread: ADS1248, ADS1118, ADS1115, ADS9110, ADS8881, ADS8860, ADS7042

Hello Team,

Our customer requires to strictly managing the ADC sampling timing. Is there any ADC device which could meet either of the following function/spec ?

- Samples the input data at the moment applying a timing pulse externally.

- Samples the input data after a fixed time delay after applying a timing pulse externally.

I am asking for the sample rate and resolution requirements. Could you please advise us if TI has such device or not ?

Best Regards,

Kawai

  • Takushi-san,


    Many devices have timing that is exact in terms of when data comes out. If you look at Tables 15 and 16 of the ADS1248 datasheet you can see the time in which it takes to get a data out. This of course assumes that you have an oscillator clock of exactly 4.096MHz. In the first table, the timing is for a START pin used to initiate the conversion. In the second table, it is the timing for changes in the configuration register. Many of data converters will have this type of exact timing. This might work for you customer.

    However, there are reasons why this type of data converter might not work for your customer. Most precision data converters in our product line are delta sigma type data converters. In this case, the data that comes out is close to an average of the input from the start of the conversion to the end of the conversion time. If your customer needs a conversion with a sample-and-hold for the data at the moment of the start of the conversion, then this type of converter will not work for them. I don't think any of our devices in the 24-bit range have this.

    I think we would want to know the data rate, resolution, and the nature of their sampling to get an idea if we have what they need. We'll probably need some description of their system and to help them make a selection.


    Joseph Wu
  • Hello Joseph-san,

    My apologies for my delay. Thank you for your reply.
    Customer requirement specification is below.

    - Sampling Rate : 860SPS
    - Resolution : 15bits
    - Input signal : single end LVCMOS
    - Input Range : 0 to 4.096V

    Customer would like to use the ADC in single shot operation with fastest sampling after single control pulse. They will keep the device in sleep (low power mode) when not used.

    Could you please advise us your recommendation ?

    Best Regards,
    Kawai
  • Kawai-san,


    Based on the 860 SPS data rate, it sounds like your customer is interested in the ADS1115 or the ADS1118. The first device uses I2C while the second uses SPI.

    These devices all have the basic features that you describe, including the ability to shut it down when not in use.

    I would however, be concerned about the data rate. In your first post, you mention strictly managing the sample timing. In these devices, there is an internal oscillator which does have some variability in the internal clock rate. Both of these devices do have an 860 SPS data rate, but it can be off by +/-10%.

    If there's more information about what the customer would like to do, I'd be interested in hearing about it. However, it's likely that the either the ADS1115 or the ADS1118 will work for your customer.


    Joseph Wu
  • Hello Kawai-san

    Looking at your requirements, a SAR ADC may also be a good fit for your application:
    1) In a typical SAR ADC, an external CONVST or CSz signal is used to control the sampling instant for the device. The device holds the input signal value at the rising or falling edge (device dependent) of the sampling control signal after which it goes into conversion phase to provide a digital output.
    2) Since the sampling control is user controlled, it can be applied after any time delay. In some new ADC architectures, the device consumes zero power after completing a user initiated conversion. The zero power state is maintained until the next sampling control is initiated. This results in significant power savings if a device is used at a low sampling rate.

    Some of our new SAR ADC devices support the above described power scaling feature, namely below:
    1) 18 bits --> ADS8881/3/5/7 ; ADS9110
    2) 16 bits --> ADS8860/1/2/3/4/5/6/7
    3) 12 bits --> ADS7042/3/4

    Please let us know if you have any follow up questions in this regard.

    Thanks
  • Hello Joseph-san, Vinay-san,

    Thank you for your advices. I will promote these devices and ask for their feedback. Please allow me to ask you for your help when we have further questions or requirements.

    Best Regards,
    Kawai