This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AFE4300 I and Q code range

Other Parts Discussed in Thread: AFE4300

Hi there,

I'm have a custom board with ARM MUC on board with AFE4300 and I was able to get single capture to function, however I ran the single capture while the AFE4300 is not connected to any resistor network other than the 10M DC feeback resistor between the current in and out pins (measuring open circuit), I was hoping to get a maximum reading of I code while its open circuit, I got close to 0 hex every time I do single capture with open circuit.

Whereas on the GUI supplied by TI under "ADC capture & analysis" tab I setup the AFE4300 to do 8 sample measurements with open circuit on the EVM board, the code it returned was around 19300, and short circuit measurements returns a very small value around 30. 

can you tell me what is this code that the GUI returns? is that hex from the ADC register being converted to decimal or ?

What is the relationship between the I code and the resistance?