Is it possible to achieve a dynamic range of 160 dB using two ADCs? One ADC channel would have a gain of 1, while the other ADC channel would have a much higher gain.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Is it possible to achieve a dynamic range of 160 dB using two ADCs? One ADC channel would have a gain of 1, while the other ADC channel would have a much higher gain.
Hi Art
If a high precision SAR ADC architecture is used, the gain for the other channel needs to be somewhere 60dB (1000) or 80dB (10000). It may be little easier to synchronize the two ADC channels with the SAR architecture.
A Delta-Sigma ADC architecture will provide a much higher dynamic range so it will reduce the front end gain requirements. What is your sampling rate requirements for this system.
Thanks