This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

RD-195 current sensor selection

Hi

I am evaluation the the RD-195 Arc detection circuit board, question as below,

1. How does the board judge the Arc?

2.How to select the coil of current sensor?

  • Hello Mark,

    The RD-195 works by dynamically filtering out potential interfering signals, such as inverter switching noise, and then looks for an increase in the overall noisefloor of the system.

    The current transformer should be selected such that it will not saturate with the maximum DC current that could occur, and it should transfer the frequency range of 20kHz to 100kHz to the secondary.

    Regards,

    Chris O