Other Parts Discussed in Thread: ADC3222
Hi
Let me three questions ADC3222.
Q1) How to print the CUSTOM PATTERN in CHA or will correct in the following order ?
1. address 0Eh = bit[7:0] is set to CUSTOM PATTERN
2. address 0Fh = bit[7:4] is set to CUSTOM PATTERN
3. address 09h = 02h (Test pattern aligned)
4. address 0Ah = 06h (Custom pattern)
5. address 06h = 02h (Test pattern enable) Do you have operations to add?
Q2) address 0Ah [3-0]: when set to "0100", 1LSB will increase every 4clock cycle.
What is the cause? (Do you CLK DIV(27h) is involved?)
Q3) Data sheet(SBAS672A)page54 Here, the following description is written.
FLIP BITS : 1= MSB comes out first, sequence is 13,12,11, and so forth.
ADC3222 is so 12Bit, "11,10,9" is I think correct. Does this idea is wrong?
Best regards