Other Parts Discussed in Thread: DAC101C085
Hello guys,
Our customer would like to know what is the minimum/maximum time of DAC101C085 SDA/SCL input signal rising/falling.
I checked the device datasheet. Then I found several parameter names about SDA/SCL rise/fall time on page 9.
But I have a few questions about the parameters.
Q1. Are parameter trDA/tfDA/trCL/trCL1/tfCL for input signal or output signal?
Q2. If the parameters are for input signal, what is rise/fall time of SDA terminal in output mode? (I think it depends on pull up resistor value.)
Q3. Our customer uses the fast mode of I2C and open drain buffer to driver SDA/SCL bus. According to the datasheet, in case of the fast mode,
SDA input signal rising time must be between 20 + 0.1Cb ns (min) and 300ns (max),
SDA input signal fallng time must be between 20 + 0.1Cb ns (min) and 250ns (max),
SCL input signal rising time must be between 20 + 0.1Cb ns (min) and 300ns (max),
SCL input signal fallng time must be between 20 + 0.1Cb ns (min) and 300ns (max).
Our customer controller controls DAC101C085 SDA/SCL using open drain buffer.
No any other I2C device is connected to the I2C bus. Their current SDA/SCL falling time is about 10ns.
Do they need to add some capacitance to reduce the falling time to meet the datasheet value?
Your comment would be much appreciated.
Thank you and best regards,
Kazuya Nakai.