Other Parts Discussed in Thread: ADS1299
I am using ADS1299 with arduino.
Although, arduino outputs high level digital signals as 5V.
Checking ADS1299 datasheet, it says the maximum input voltage for logic level high is DVDD + 0.1
Since I am using a 3.3V digital supply, this means that my maximum value for logic level high is 3.4 V.
So my question is: Is it a problem to use arduino, even though its output signals are 5V when in high level?
Thanks