Hello guys,
I have an ADS1293EVM board, I removed the resistors that connect the MSP to the ADS, so I can use the spi bar to communicate with another microcontroller (which I have more experience and my company have being working with for another projects).
The problem begun when the ADS datasheet (pg. 37, figure 29), presents the SPI protocol and it states that during the 8th clock cycle 2 bit transactions happen (one at the raising and other at the falling edge of SCLK) . I would like to know if that is correct, because I am not able to program the chip correctly, even though I can read the default register values, but the sample rate does not respond to my commands.
Any help will be very much appreciated.
Att, Felipe.