Other Parts Discussed in Thread: ADS52J90, ADS6442
Question: Is the max and min input voltages for the ADS6442 Vcm+/- 0.5V as it is on the ADS52J90?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
Yes, as described on page 48 of the datasheet:
The INP and INM pins have to be externally biased around a common-mode voltage of 1.5 V, available on VCM pin
13. For a full-scale differential input, each input pin INP, INM has to swing symmetrically between VCM + 0.5 V
and VCM – 0.5 V, resulting in a 2-VPP differential input swing.
Regards,
Richard P.