This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

8x AFE4490 Power Supply

Other Parts Discussed in Thread: AFE4490

Hi there,

on the Evaluationsboard AFE4490 i have two Power Supplies  +5V(LED_DRV_SUP and TX_CTRL_SUP) and +3V3(RX_DIG_SUP and RX_ANA_SUP).

On my board there are three Supplies that i can use to drive the Ics:

a- +5V_ANA for LED_DRV_SUP and TX_CTRL_SUP 

b- +3V3_ANA for RX_ANA_SUP

c- +3V3_DIG for RX_DIG_SUP

My questions are:

1-Voltage

How do i supply 8x AFE4490 so one cannot influence the other? Ferrite or inductor?

2- Current

In worst case when all 8 ICs run at maximum power consumption, what would be the Current consumption from +5V_ANA, +3V3_ANA and +3V3_DIG?

On the Datasheet it says Input Current momentary at +-50mA, but what if i drive the LEDs with 200mA?