For the ADS7951, I need to capture all channel with auto increment starting from Ch0. During this capture, the range settings will not change for each channel.
As I understand the specification: Auto-2 mode is entered by programming the first 3 frames with SDI contents as described in Table 5. At the end of 3rd frame, the ADC enters Auto-2 mode. From 4th frame onwards I do not need to send any data on SDI (continued operation mode) and SDI should be low. In this mode, the ADC will auto increment channel with each frame.
What I am seeing on the bench is a little different: In my case, I only need to program one frame, not three as described in the specification. I perform the same procedure as outlined above, but instead of three frames, the ADC seems to enter Auto-2 mode only after one frame. From 2nd frame onward I do not need to send any data on SDI and SDI is low. In this mode, it the ADC appears to be auto incrementing channel with each frame. Is there an explanation as to why only one frame seems to get the device into Auto-2 mode VS the three frames described in the specification?