Other Parts Discussed in Thread: ADC16DV160
Dear All,
Let me confirm it about dBFS specifications of ADC16DV160.
Please refer to the attached data.
"ADC16DV160_dBFS_Data@10MHz.pdf"
This is the data that our customer performed the FFT measurement of ADC16DV160 on their system.
Our customer is concerned about dBFS growing big in the range of low frequency from -90dBFS.
【Our Customer request】
dBFS < -90 :Pass
dBFS > -90 :Fail
With most cases, dBFS satisfies the request of the customer.
But, According to the part of the red letter of the table,
in the case of Fs=305Hz, FS-4dB, "-95.5dBFS" was confirmed.
(It is a value near "-90dBFS".)
May the dBFS specifications of ADC16DV160 become -90dBFS in the range of low frequency?
Best Regards,
Tsuguhiko Asai