Other Parts Discussed in Thread: ADS1244
Hello,
I m using ADS1244 for voltage reading.
If i use
AVDD=5V
DVDD=3.3V
Ref (+)positive = 2.5V
Ref (-)negative= 0V.
AINN=0V
Question 1 ) AINP range should be +/- 5V. Is this correct?
or AINP is limited by AVDD/2 ? (Datasheet states +/- 2 Vref)
Question 2) according to the setting, it should output 7F FF FF for AINP=5V?
and FF FF FF for AINP = -5V ????
Question 3) This setting for ADS1244 is capable of measuring from -5V to +5V ?