This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DAC37J84 JESD204B SYNC Setting?

Other Parts Discussed in Thread: DAC37J84, DAC38J84

DEARS.

DAC37J84 related to need help.

Our customer would evaluate JESD204B Link by FPGA-DAC37J84.

Could you please check the status below?

Q1. The reason that JESD204B SYNC does not work?

Q2. Increasing the 0.9V power to 0.95V reason JESD204B SYNC  to work?(VDDIG09, VDDAC09,VDDCLK09, VDDT09)

DAC37J84 JESD204B Setting Value

Line Rate : 5000Mbps

SYSREF :    7.8125M

DACCLK :    1000M

LMFK :     L=4, M=4, F=2, S=1, K=16

Frame CLK, Sampling CLK: 250M

LMFC: 15.625M

Serdes Line0, Line1, Line2, Line3

Please let me know there is DAC37J84  in JESD204B interface architecture.

Best Regards,

  • Henry,

    The procedure for the DAC37J84 SYNC are the following:
    1. upon powering up, the 0x4A register init_state = 2b1111 and jesd_reset = 2b0, the LVDS SYNC pair should be logic HIGH
    2. program 0x24 and 0x5C accordingly to allow SYSREF pulses to be registered in the state machine.
    3. program all the JESD204B and DAC parameters.
    4. write 0x4A register = init_state = 2b1111, jesd_resetn = 2b1
    5. write 0x4A register = init_state = 2b0000, jesd_resetn = 2b1.
    6. The JESD204B block is initialized at this point, upon issuing a sysref pulse, the LVDS SYNC pair should be logic LOW, requesting CGS from JESD204B transmitter.
    7. upon completion of CGS and stage to enter ILA, the SYNC should be logic High.

    Please help clarify which stage the SYNC does not work.

    Also, you mentioned elevating VDD from 0.9V to 0.95V will allow SYNC to work. Is this measured on the device pin after PCB trace loss and power filters? Please note that VDD draws sufficient current, and any drop in voltage due to resistance loss will cause the voltage threshold to drop below recommended value. I would advise the customer to measure the voltage during operation near the device pin as much as possible to check the actual voltage level. They may use the ATEST feature in config27 if needed to measure internal nodal voltages.

    -Kang
  • DEAR. Kang

    There are answers for the questions.
    Customers assemble the five board.
    Two boards are Good operation.
    JESD204B Interface is not operating in the three boards.

    I doubted the SMT and DAC37J84 has a SWAP testing.
    The test results were the same.


    What are the ways to solve the problem?

  • DEAR. Kang

    There are answers for the questions.
    Customers assemble the five board.
    Two boards are Good operation.
    JESD204B Interface is not operating in the three boards.

    I doubted the SMT and DAC37J84 has a SWAP testing.
    The test results were the same.


    What are the ways to solve the problem?
  • Henry,

    Please clarify your question. I have asked for the symptoms of JESD204B failures and the DAC38J84 alarms in the previous posts, but I have not received any feedback. At this point, I am not sure how to proceed.

    There are two good boards with good operation. Please advise the error reported on the DAC registers config100 to 108 and also the process of failure before we can proceed any further.

    -Kang