Hello
I am trying to use the lead off detection function with the ADS1299 PDK.
Before this, I confirmed that this kit could measure EEG properly.
But I am not sure whether I can test lead off detection function to measure the impedance of the individual electrodes.
On the kit, I will connect the (+) input connector to the (-) input connector, which is then jumped to the ground connector.
If the 6nA current is injected to the input wire, voltage drop across two connectors would appear, I think.
(In this case, about zero resistance would appear. Is it right?)
Could you give me some tips about setting up the register on the GUI?
Thanks ^^