Other Parts Discussed in Thread: ADC34J22, DEV-ADC34J22
Thanks for your time. I have recently bought this ADC34j22 EVM board. It supposed to be DEV ADC34j22 but I have mistakely ordered ADC34j22 EVM. Anyway I have lots of questions and hoping for your helps.
1- How can I access to the converted digital value of this board? Is the FMC connector the only way? Is there anyway to receive the digital output and connect to GOIP pins of FPGA boards?
2- I have to make a feedback loop for some application and need to convert analog to digital to modify in FPGA. My analog input is a kind of special waveform. I have a square input with 100 Hz input frequency and 80 ns duty cycle. Every 10 ms I have 80 ns pulse.
Is it possible for this ADC34j22 EVM board to somehow convert this value to digital to modify in FPGA.
Appreciate for your instructions.
P.S: I have attached the waveform shape also. Square waveform final.doc