Hi,everyone.I nearly used AMC7812b and CC3200 to design a remote sensor system. I have read the AMC1812b' s reference. I saw the DAC source current and sink current is +10mA and -10mA respectively. So is that means each of the DAC have that drive ability and 12 DAC can work together totally output 120mA current ? However ,if that's true is that conflict with the device power consumption of 95mW ?