Other Parts Discussed in Thread: AFE4404, AFE4400
I am unable to communicate with the device. I installed the GUI after the installation I plugged in the USB. Windows 8 immediately recognized it as a virtual serial port (I have used the PC for other development on the MSP430 and as well as the LM4f120) It did not lable the port as afe... The port number was 6, which I raised to 30. Still to no avail. I tried to update the driver by pointing to the TI folder as suggested but windows claims that the driver is the lastest version.
Please advise.