This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS1298 don't express any coherent signal

Other Parts Discussed in Thread: ADS1298

Hi, 

I'm using ADS1298 in a project and I tried to test it, but the converter do not send a coherent signal. The only I have are random spikes (maybe white noise) on output. I checked SPI and it works fine. This is my configuration vector:

const byte adsConfigRegs[] = {
    0x06, // Config 1 - low power, daisy-chain, 1kS
    0x13, // Config 2
    0xc0, // Config 3
    0x00, // LOFF

    0x15, // CH1SET 11
    0x15, // CH2SET 10
    0x15, // CH3SET 10
    0x15, // CH4SET 11
    0x15, // CH5SET 11
    0x15, // CH6SET 11
    0x15, // CH7SET 11
    0x15, // CH8SET 11

    0x06, // RLD_SENSP
    0x02, // RLD_SENSN

    0x00, // LOFF_SENSP
    0x00, // LOFF_SENSN
    0x00, // LOFF_FLIP

    0x00, // LOFF_STATP
    0x00, // LOFF_STATN

    0x0f, // GPIO
    0x00, // PACE
    0x00, // RESP
    0x00, // Config 4
    0x00, // WCT1
    0x00 // WCT2
};

With this configuration, I put it in RDATAC mode and the triggered interrupt generated by DRDY pin is handled and all output data is read. When I change the switch among the different input signals I can notice some change on output signal behavior, but still a messy signal.

I can send you more datails from my configuration and code.