I am trying to interface DDC112 with ATMEGA32 micro controller but no dvalid signal is coming from DDC112.The steps are given below:
1. AVdd and DVdd are tied up together to 5V supply.
2. 7.5MHz is given to DDC112.
3. TEST pin is high and CONV is toggling 1ms time interval.
4. Range0 to Range2 pins are at logic high level.No external capacitor connected.
5.DXMIT at high logic state and DCLK,DOUT at low logic state.
In this case DVALID signal coming from ddc112 is always at high logic state.Please help me out .....