Other Parts Discussed in Thread: ADS8555
From the data sheet of ADS8555 ADC : channel gain error = ±0.25%FS typical value ( ± 0.75%FS max value)
this value is an absolute value for one independent channel , what about differential measurement between two channels of one pair (matching)
- what's the value between any two input channel of any of SAR ADC ?
- what's the value between any two input channel of any pair of SAR ADC (matching) ?
note : the gain error of ANALOG DEVICES AD7656 (compatible with ADS8555) is defined in datasheet :
full-scale error : ±0.75%FS max ( ±0.22% FS typical)
matching error (between 2 channel) : ±0.35%FS max