Hi Team,
I heard my customer saw CLKOUT pin outputs 480kHz despite he used 8MHz crystal on his board.
Is it possible case if he mistake to select a suitable crystal for AFE4400 or load capacitance?
Best Regards,
Yaita / Japan disty
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Team,
I heard my customer saw CLKOUT pin outputs 480kHz despite he used 8MHz crystal on his board.
Is it possible case if he mistake to select a suitable crystal for AFE4400 or load capacitance?
Best Regards,
Yaita / Japan disty
Kensuke,
If the customer is using his own board, then yes it is possible. They can verify the pins using our EVM and the settings they have.
Hi Amy-san,
Thank you for your comment.
The ESR(max:500Ω) of my customer's crystal seems larger than that of recommended in the following forum.
http://e2e.ti.com/support/applications/high_reliability/f/30/t/306018
I will inform the forum to my customer.
Best Regards,
Yaita