I'm attempting to use leadoff detection to measure impedance using the ADS1299. My main issue is actually getting it to work. With the 1299 connected to the motherboard, I can do leadoff detection perfectly. Everything works just as advertised. However, when I hook up the 1299 to my device which communicates through SPI, it seems that only Channel 1 works. Channel 1 will do leadoff detection, but other channels only produce a slowly oscillating square wave. The registers I used for the motherboard are here, captured using TI's provided software. Our registers are exactly the same except for the last bit of Config 3, which appears to be read only and will not flip. I feel like there's some significance there, but I can't quite figure out what.