Other Parts Discussed in Thread: LMK04828, ADS54J66EVM
Hey guys,
I'm trying to use the ADS54j66EVM with the onboard LMK04828 Clock Chip in the Clock distribution mode as described in section 5.1.2 of the ADS5XJ6X Evaluation Module User guide. I've removed the JP2 jumper and inserted a 122.88MHz clock signal into CLKIN(J12) of the board and loaded the LMK_Config_External_Clock Configuration file in the ADs54Jxx GUI to test if the PLL2 can be locked in the same way with the external clock. However, when I do this PLL2 does not lock. I am curious on how the external LMK04828 Clock Distribution mode is used and whether or not the external clock(fed into J12) replaces the on board vcxo which can be stepped up using the PLLs in the same manner as using the on board vcxo?
Thanks in advance for the help,
Brian