Hello - I have a question regarding the recommended output load of the TLV5632. The datasheet calls out a maximum capacitance of 100pF and a minimum resistance of 2kohm. Could the part be damaged if the loading capacitance is on the order of 200pF to 10nF? I'm seeing a couple of our boards that use this DAC become either completely inoperable or the output offset and amplitude is completely different than what is being commanded through the SPI bus. Is it recommended to use a low capacitance input amplifier to act as a output buffer for this part? Thank you.