Other Parts Discussed in Thread: ADS8318
I am looking at using the ADS8318 in CS mode, 3 wire without busy indicator. The rev A spec SLA568A gives a minimum acquisition time of 600ns, but for 16 bit data clocked on a 50MHz max SPI clock, the data acquisition should be 320ns (16 * 20ns) plus the tEN output enable time of 15ns, or 335ns. Why does the spec say 600ns, almost twice as long? I feel like I am missing some extra delay parameter, but there's nothing of the right order of magnitude in the table, and nothing shown in the timing figure 46 to explain a missing 265ns. Please help - thanks!