Hi,
We are having a custom board in which DM6446 is connected to THS8200 to get SVGA display on monitor.
16bit YCbCr is interfaced to THS8200 with FID pin connected to GIO3/LCD_FIELD_B0.Color space conversion is enabled since YcbCR to RGB conversion is required and I have programmed the color space convesion registers withe values specified in the example
Register programmed values are
|
Register Address |
Value |
|
0x3 |
0x01 |
|
0x4 to 0x19 |
0x00 |
|
0x19 |
0x03 |
|
0x82 |
0x5b |
|
0x1c |
0x03(20 bit -4:2:2 YcbCr mode) |
|
0x1d to 0x1f |
0 |
|
0x20 to 0x24 |
0 |
|
0x36 |
0x80 |
|
0x37 |
0x01 |
|
0x38 |
0x87 |
|
0x25 |
0x40 |
|
0x26 |
0x28 |
|
0x27 |
0x40 |
|
0x28 |
0x58 |
|
0x2a |
0x58 |
|
0x2b |
0x00 |
|
0x2c |
0x00 |
|
0x2f |
0x28 |
|
0x30 |
0 |
|
0x34 |
4 |
|
0x35 |
0x20 |
|
0x39 |
0x22 |
|
0x3a |
0x74 |
|
0x3b |
0x74 |
|
0x41 |
0x40 |
|
0x42 |
0x40 |
|
0x43 |
0x40 |
|
0x44 |
0x53 |
|
0x45 |
0x3f |
|
0x46 |
0x3f |
|
0x47 to 0x49 |
0x40 |
|
0x4a |
0xfc |
|
0x4b |
0x44 |
|
0x4c |
0xac |
|
0x4d |
0x91 |
|
0x4e |
0x91 |
|
0x4f |
0xff |
|
0x70 |
0x80 |
|
0x71 |
0x00 |
|
0x72 |
0x01 |
|
0x73 |
0x05 |
|
0x74 |
0x00 |
|
0x75 |
0x1 |
|
0x76 |
0x00 |
|
0x77 |
0x7 |
|
0x78 |
0xff |
|
0x79 to 7c |
0x00 |
|
For Color bar |
|
|
0x2a |
0x58 |
|
0x2b |
0x40 |
|
0x38 |
0x86 |
|
0x3c |
0x20 (width of each color bar) |
|
0x3 |
0x23 |