Hi all
Would you mind if we ask AMC1305M25?
<Terminal processing of NC pins on the datasheet>
-1pin : This pin can be connected to AVDD or can be left unconnected
-5pin : This pin can be left unconnected or tied to AGND only
-6, 10, 12pin : These pins have no internal connection (pins 10 and 12 on the AMC1305Mx only)
-15pin : This pin can be left unconnected or tied to DVDD only
About 1 pin, we recognioze that it is OK to connect to AVDD.
So, why are terminal processing of NC pins different in different pins?
We think all of NC pins are no internal connection.
Kind regards,
Hirotaka Matsumoto