Is it possible to obtain the source code for the TSW308x GUI? I would like to be able to load the TSW3084EVM parameters directly from file. Althought the GUI has a file load option it doesn't seem to load all the parameters that I need (i.e. device selection, PLL frequency, and NCO Fsample are all not set). Failing that can you provide a version of the GUI that does configure all of the parameters from a setup file?