Other Parts Discussed in Thread: ADS1262
Hi there. I am using the ADS1262 with GPIO6 (AIN9) and GPIO7 (AINCOM) configured as outputs. I can set the output on each pin correctly by writing to register 0x14, but I always read back 0x00 regardless. I was confused because the note in the "Description" column in Table 47 says "Configured as an output, read returns the register value". I believe there is a mistake in the note but need confirmation. To me, it seems the note should read:
"Configured as an output, write sets the register value only.
Configured as an input, read returns the register value."
Please clarify.
Thanks very much!